Failed to Open. Plug DEMO board into PC via USB cable.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failed to Open. Plug DEMO board into PC via USB cable.

1,497 Views
rodrigocorrêa
Contributor II

Hello.
I'm having trouble to connect my DEMOEM board to the computer through the Terminal Utility.

 

I'm using the DEMOEM board for COLDFIRE MCF51EM256. I can download a program to the broard, written in the CodeWorrior 6.3 and debug it; All drivers seems to be correctly installed: in the device manger, I can see the Jungo Connectivity and PEMicro USB ans Serial interface (i00) and (i01); I am using Windows 10.

 

Can anybody help me?

Labels (1)
0 Kudos
Reply
1 Reply

1,301 Views
miduo
NXP Employee
NXP Employee

Hi,

What is your setting of the Terminal Utility? There should have no hardware issue because you had connect the board success, so it is really an software issue.

0 Kudos
Reply