Error in MCF52259RM and MCF52259DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error in MCF52259RM and MCF52259DS

1,724 Views
daverj
Contributor I
In both the MCF52259RM.pdf and MCF52259DS.pdf the table showing the pins list RTC_EXTAL as pin 33 and RTC_XTAL as pin 34 on the 144 LQFP. However the FB_AD7 and FB_AD8 signals are also listed as being those pins in a different part of the table.

In the package diagram for the 144 LQFP in the MCF52259DS.pdf the RTC clocks are shown as pins 13 and 14. Also on the schematic for the M52259EVB.

So I think the ones in the table of pins are wrong in both documents.

Both documents were downloaded from the site this week.

Labels (1)
0 Kudos
Reply
1 Reply

1,097 Views
J2MEJediMaster
Specialist I

I'll pass this on to the docs people and see what they say.

 

---Tom

0 Kudos
Reply