アクセスしようとしているメッセージは完全に削除されました。
I'm working with MCF51QE128 and CW6.3
If I'm not using any dynamic memory allocation, could I eliminate heap? I mean define heap size as 0x0000 so I can gain more RAM
Thanks in advance!
Hello
Yes this is possible defining a heap_size of 0 bytes should be supported.
CrasyCat
Thanks!
I was near my RAM limit, now I've got 1K more!
I have a similar question, I don't use malloc() but my heap is defined differently, can I just remove all references to __HEAP* from the .LCF?
___FLASH = ADDR(.bootcode); ___FLASH_SIZE = 0x00080000; ___SRAM = 0x20000400; ___SRAM_SIZE = 0x0000FC00; ___VECTOR_RAM = 0x20000000; ___IPSBAR = ADDR(.ipsbar); ___SP_SIZE = 0x2000; # 8k ___HEAP_START = .; # Store after sections above (.bss) ___HEAP_END = ___SRAM + ___SRAM_SIZE - ___SP_SIZE; ___SP_END = ___HEAP_END; ___SP_INIT = ___SP_END + ___SP_SIZE; ___heap_addr = ___HEAP_START; ___heap_size = ___HEAP_END - ___HEAP_START ; __SP_INIT = ___SP_INIT; # http://forums.freescale.com/freescale/attachments/freescale/CWCFCOMM/3435/1/TN268.pdf ___mem_limit = ___HEAP_END; ___stack_safety = 16;