Digital  2 wire 4-20mA conversion to voltage modulated signal

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Digital  2 wire 4-20mA conversion to voltage modulated signal

1,335 次查看
Dave_W
Contributor I

Hi

 

I need to use a digital single axis accelerometer with capacity to go up to a few hundred g's.  The only decent ones I've been able to get hold of are the ADXL180's from ADI.  However my project is using the MCF51JM128 so I need to find a way to interface with the device as it uses a 2 wire digital 4-20mA interface.

 

Now from what I've read I can use a precision resistor and sample the voltage across the resistor through the ADC but then I must do a bunch of programming to convert that into something useful.  I don't mind doing the work but I want to know if there is a better solution then bit banging a comms interface.  Are there any IC's out there that convert it to a standard interface like SCI/SPI/I2C?

 

Thanks in Advance

 

Dave Wright

标签 (1)
0 项奖励
回复
1 回复

1,059 次查看
FridgeFreezer
Senior Contributor I

Surely with the correct resistor values you should be able to do it on a normal digital IO pin?

0 项奖励
回复