DSPI as GPIO register/pin relationship in MCF5445x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DSPI as GPIO register/pin relationship in MCF5445x

1,082 Views
w_wegner
Contributor III

Hi all,

 

I am trying to debug some things by bit-banging the DSPI pins on my board.

 

While doing so, I think I found a problem in the documentation of the DSPI Pin Assignment Register PAR_DSPI (page 16-28/PDF 368) of MCF54455RM Rev. 5.

 

The documentation reads:

Bit 0: PAR_SCK

Bit 1: PAR_SOUT

Bit 2: PAR_SIN

 

But I think it should be

Bit 0: PAR_SOUT

Bit 1: PAR_SIN

Bit 2: PAR_SCK

 

Can anybody confirm this, or do I have to debug further?
(I also have a simple serial flash connected to DSPI and can access it using the DSPI peripheral, so the pinout in our layout should be correct.)

 

Best regards,

Wolfgang

Labels (1)
0 Kudos
Reply
1 Reply

530 Views
w_wegner
Contributor III

Hi again,

 

now I found where this confusion originates from:

 

The pin/GPIO index is correct in the  external signal description (pp. 2-2ff, 16-4ff), but the mapping in the corresponding PAR_xxx register is different for some units (namely, SSI and DSPI, pp. 16-28f, 16-34).

 

It would be nice if freescale could comment on this (and leave a comment in the datasheet) if this different mapping is really intentional or to correct the PAR_xxx bit definitions to clarify this part of documentation.

 

Regards,

Wolfgang

0 Kudos
Reply