DEV5213CF p&e evaluation board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DEV5213CF p&e evaluation board

2,680 Views
uni_student
Contributor I
i recently bought the evaluation board from p&e micro, i can get provided demo programs to run on the controller but am finding it hard to include all the neccessary c definitions for even basic functions. this is making it hard to write my own code as i cant even seem to set certain pins as inputs, i am currently trying to create a new program from an assembly level template but this is not included in the evaluation version of the software.
 
anyone have the nesassary c header files i need to include?
or does anyone know how i can create/change an assembly level project?
 
Help would be apreciated
 
thanks andy
Labels (1)
0 Kudos
Reply
2 Replies

1,719 Views
Marcia
Contributor I
Hi Andy,
 
You maybe want to try submitting a service request on P&E directly. I'm sure those guys will point you in the right direction. I'm not familiar with the tool-chain you're using, and from the lack of response to your query here, I guess that the guys on this forum are not, either.
 
Marcia
0 Kudos
Reply

1,719 Views
uni_student
Contributor I
thanks, i got the chip configured how i wanted. thanks for the reply anyway
0 Kudos
Reply