ColdFire bdm troubles

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ColdFire bdm troubles

2,278 Views
Ricardo_RauppV
Contributor I
 
Hi folks !!
 
I´m using MCF5211 and its P&E bdm to debug it (with Codewarrior 6.3 , linker 6.2).
I have 2 questions I cannot solve yet ...I hope you can help me ...
 
a)
When running the debugger, I have frequently a problem releted to "loss of communication" and so I need to close the debugger screen and restart it (F5) to run again ....
 
b)
A second and very strange thing is..when I get close quckly to the target, the debugger screen (and the bdm..) stops and show a Vector 0 position, as it had lead to such position due to some reason.
It happens inside our lab, a very free of noisy environment...and free of ghosts (I hope...)
I have experienced it a lot in 9S12 / 08 bdm ....
To solve this last one I believe I must consult a priest .. :smileyhappy::smileyhappy:
 
Could soneone help me ?
 
 
Ricardo Raupp
Labels (1)
0 Kudos
Reply
1 Reply

1,309 Views
jholler
Contributor I
Hello Ricardo,
 
With respect to item a).  We found this to be a problem when dealing with the 68HC12 and its BDM.  Are you using a watchdog timer?  If so, has it been turned off.  Having a watchdog timer turned on will interfere with BDM communications.
0 Kudos
Reply