Bootloader V3_2 for Coldfire V2 (MCF52259) on windows 10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bootloader V3_2 for Coldfire V2 (MCF52259) on windows 10

1,977 Views
Krokodyl
Contributor I

Hello, I'm using USB MSD Bootloader V3_2 for Coldfire V2 (MCF52259). Now I have problem with enumeration in OS windows 10. Is there any solution of this problem? Thank you. Jiri

Labels (1)
0 Kudos
Reply
3 Replies

1,643 Views
TomE
Specialist II

Then the solution is to create a Windows 7 VM (or even an XP VM) specifically to support that debugger and your development environment.

Tom

0 Kudos
Reply

1,643 Views
miduo
NXP Employee
NXP Employee

Hi,

I am afriad that the USB MSD bootloader for ColdFire does not tested under the WIN 10. Have you tried with Win 7?

0 Kudos
Reply

1,643 Views
Krokodyl
Contributor I

Yes, I did. There is no problem under WIN 7.

0 Kudos
Reply