Bootloader V3_2 for Coldfire V2 (MCF52259) on windows 10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bootloader V3_2 for Coldfire V2 (MCF52259) on windows 10

1,969件の閲覧回数
Krokodyl
Contributor I

Hello, I'm using USB MSD Bootloader V3_2 for Coldfire V2 (MCF52259). Now I have problem with enumeration in OS windows 10. Is there any solution of this problem? Thank you. Jiri

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,635件の閲覧回数
TomE
Specialist II

Then the solution is to create a Windows 7 VM (or even an XP VM) specifically to support that debugger and your development environment.

Tom

0 件の賞賛
返信

1,635件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

I am afriad that the USB MSD bootloader for ColdFire does not tested under the WIN 10. Have you tried with Win 7?

0 件の賞賛
返信

1,635件の閲覧回数
Krokodyl
Contributor I

Yes, I did. There is no problem under WIN 7.

0 件の賞賛
返信