Backup Watchdog

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Backup Watchdog

1,899件の閲覧回数
Dekabrist
Contributor I

Hello, all

 

My board run under BDM and Backup Watchdog Timer init with Processor Expert bean. But, when I break debug (stop Run) Backup Watchdog Timer NOT reset MCU and I read WCNTR = 0000, even when my programm write 0x5555 0xAAAA to WSR. My configuration:

CLKMOD[01] = 01 (CLKMOD0 pin have pullup resistor, XTAL pin NOT have pullUP resistor)

BWCR (CLOCK MODULE) = 0x00 - 32 MHz from bus

WCR = 0x0003

WMR = 0xFFFF - 8388,48 ms timeout

 

Init function:

 

void Wtm1_Init(void)

{

  /* WMR: WM=0xFFFF */

  setReg16(WMR, 0xFFFFU);              

  /* WCR: ??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,STOP=0,WAIT=0,DOZE=0,??=1,EN=1 */

  setReg16(WCR, 0x03U);                

}

 

Can I check software reset in the debug mode?

 

P.S. I use CW version 5.9.0 build 5293

 

Thank for answer

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,728件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Sergey,

The ColdFire BWT is good for production application but not good for debugging mode.  The BWT clock continues clocking even when you hit a breakpoint (which stops the core but it not the same as implementing a STOP instruction).

You could use the internal (slower) clock rather than the 32MHz to increase the timeout period.

Regards,

David

0 件の賞賛
返信

1,728件の閲覧回数
Dekabrist
Contributor I

Hi David

I activate toolbutton "break " in the debug mode and wait more than BWT timeout - BWT must reset MCU under this conditions? I make sure that my BWT work.

Sergey


0 件の賞賛
返信