Anybody using/planning MCF5329?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Anybody using/planning MCF5329?

5,024 Views
Dietrich
Contributor II
This message contains an entire topic ported from the WildRice - Coldfire forum.  Freescale has received the approval from the WildRice administrator on seeding the Freescale forum with messages.  The original message and all replies are in this single message. We have seeded this new forum with selected information that we expect will be of value as you search for answers to your questions.  Freescale assumes no responsibility whatsoever with respect to Posted Material.  For additional information, please see the Terms of Use - Message Boards and Community Forums.  Thank You and Enjoy the Forum!


Jan 2, 2006, 5:43 AM
Post #1 of 4 (46 views)
Copy Shortcut
 [ColdFire] Anybody using/planning MCF5329?  Can't Post 
--------------------------------------------------------------------------------
 
Hi all,
We are considering Dragonfire MCF5329 device for our design, looking at its enoumous peripheral support.
Has anybody started using MCF5329?
Any observations so far?
Has any vendor comeup/planning to comeup in short time with 5329 SBC?
Awaiting for such interaction with concerned party.
 
Regards,
Ameya V. Gambhir
Hardware Design
EmSyS, L&T Mumbai
Contact No. : 022-55054148 (O)
9820434120 (M)
--------------------------------------------------------------------
Jan 2, 2006, 6:19 AM
Post #2 of 4 (46 views)
Copy Shortcut
 Re: [ColdFire] Anybody using/planning MCF5329? [In reply to]  Can't Post 
--------------------------------------------------------------------------------
 
Hi,
we are developing a new COBRA Starterkit: COBRA5329. It based on
MCF5329. It will be available in february.
Regards
Dipl.-Ing. Wolfgang Elsner Entwicklung Hard- und Software
-----------------------------------------------------------------------
EMail: senTec Elektronik GmbH
Tel: +49(0)3677/4624864 | Werner-von-Siemens-Str. 6
Fax: +49(0)3677/4624866 | 98693 Ilmenau
Ameya Gambhir schrieb:
> Hi all,
>
> We are considering Dragonfire MCF5329 device for our design, looking at its enoumous peripheral support.
>
> Has anybody started using MCF5329?
> Any observations so far?
>
> Has any vendor comeup/planning to comeup in short time with 5329 SBC?
> Awaiting for such interaction with concerned party.
>
>
>
> Regards,
> Ameya V. Gambhir
> Hardware Design
> EmSyS, L&T Mumbai
> Contact No. : 022-55054148 (O)
> 9820434120 (M)
>
> --------------------------------------------------------------------
Jan 12, 2006, 8:00 AM
Post #3 of 4 (41 views)
Copy Shortcut
 Re: [ColdFire] Anybody using/planning MCF5329? [In reply to]  Can't Post 
--------------------------------------------------------------------------------
 
 
Hello,
Logic Product Development is supplying a system on module for the MCF5329 which is the standard development kit provided as a Freescale part number. For more infomration on the kit, you can check out the product link on the LPD website:
http://www.logicpd.com/eps/devkits/freescale/cdk/coldfire_sdk/
Or you can look at Freescale's website to purchase directly:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=M5329EVB&parentCode=MCF5329&nodeId=01...
The kit is a single board computer module, that is installed on a standard baseboard. The module has DDR ram, NOR flash, NAND flash, Ethernet PHY, LCD support, touch screen controller, audio codec, etc. and is a production ready product. If your end application would like to use a module, the LPD board is a possible solution.
-Kurt
--
View this message in context: http://www.nabble.com/Anybody-using-planning-MCF5329--t837197.html#a2343286
Sent from the Coldfire forum at Nabble.com.
--------------------------------------------------------------------
Jan 13, 2006, 12:09 PM
Post #4 of 4 (40 views)
Copy Shortcut
 RE: [ColdFire] Anybody using/planning MCF5329? [In reply to]  Can't Post 
--------------------------------------------------------------------------------
 
Kurt,
I would love to use one of Logic's boards but I just can't get my hands on
one, do you know were I can find one?
It looks like the processor will meet our needs but I need to evaluate the
lcd controller driving an 800x600 panel. Has any one tried a panel of that
size yet running say micro windows or another gui package?
 
-----Original Message-----
From: On Behalf Of KurtLPD (sent
by Nabble.com)
Sent: Thursday, January 12, 2006 10:00
Subject: Re: [ColdFire] Anybody using/planning MCF5329?

Hello,
Logic Product Development is supplying a system on module for
the MCF5329 which is the standard development kit provided as a
Freescale part number. For more infomration on the kit, you
can check out the product link on the LPD website:
http://www.logicpd.com/eps/devkits/freescale/cdk/coldfire_sdk/
Or you can look at Freescale's website to purchase directly:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=M
5329EVB&parentCode=MCF5329&nodeId=0162468rH3YTLC00M99287
The kit is a single board computer module, that is installed on
a standard baseboard. The module has DDR ram, NOR flash, NAND
flash, Ethernet PHY, LCD support, touch screen controller,
audio codec, etc. and is a production ready product. If your
end application would like to use a module, the LPD board is a
possible solution.
-Kurt
--
 
 
 

Message Edited by Dietrich on 04-01-2006 11:41 AM

Message Edited by Dietrich on 04-04-2006 09:41 PM

Labels (1)
0 Kudos
Reply
2 Replies

1,492 Views
RickAtPhase
Contributor I
Hi Dietrich
Did you end up using the MCF5329 in you design?
If so would you be intrested in selling the the design?
 
Rick
 
800-858-1320  x239
 
0 Kudos
Reply

1,492 Views
Alban
Senior Contributor II
Hi Rick,
 
Dietrich only copied over posts from another Freescale related forum.
The person who was thinking about the Design was:
Ameya V. Gambhir
Hardware Design
EmSyS, L&T Mumbai
The contact details are in the post, if you want to call/email the person directly to discuss.
 
Regards,
Alban.
0 Kudos
Reply