Altium model of MCF5441x processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Altium model of MCF5441x processor

ソリューションへジャンプ
2,067件の閲覧回数
danielblackmer
Contributor I

Does anyone know where I can find Altium models for this family of processors? Laying out over 250 pins by hand is doable, but it would be far better if someone else already has a model they can share.

ラベル(1)
タグ(3)
1 解決策
1,925件の閲覧回数
yibbidy
Contributor V

Hi Daniel,

I have an Altium schematic library for the parts used on the TWR-MCF5441x CPU tower module.  I converted it across from Freescale's design package that used OrCAD.  I couldn't convert the PCB files though.  I never ended up getting to the layout stage, but perhaps it will give you a hand, just need to link it the part to the standard footprint.

Shaun

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,925件の閲覧回数
danielblackmer
Contributor I

Thank you Shaun! That is tremendously helpful to me, I really appreciate it.

1,926件の閲覧回数
yibbidy
Contributor V

Hi Daniel,

I have an Altium schematic library for the parts used on the TWR-MCF5441x CPU tower module.  I converted it across from Freescale's design package that used OrCAD.  I couldn't convert the PCB files though.  I never ended up getting to the layout stage, but perhaps it will give you a hand, just need to link it the part to the standard footprint.

Shaun

0 件の賞賛
返信