AC'97 driver for the SSI bus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AC'97 driver for the SSI bus

1,479 Views
mendelbullex
Contributor III

I am currently using the linux kernel 2.6.29 with the mcf54451. I want to interface the SSI bus with a cs4202 audio codec. This chip conforms to the ac-link protocol, but I am not sure if there is driver support. It looks like there is some built in driver support in ALSA, but I'm not sure if this is true. If not I will need to get a driver for it and I have found none. Any suggestions?

Labels (1)
0 Kudos
Reply
1 Reply

1,234 Views
mendelbullex
Contributor III

OK, so it appears that the linux kernel has a driver for AC97 using PCI. Does nayone know if there is an interface that allows the mcf5445x to use this driver or another similar one with the SSI bus?

0 Kudos
Reply