AC'97 driver for the SSI bus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AC'97 driver for the SSI bus

1,475件の閲覧回数
mendelbullex
Contributor III

I am currently using the linux kernel 2.6.29 with the mcf54451. I want to interface the SSI bus with a cs4202 audio codec. This chip conforms to the ac-link protocol, but I am not sure if there is driver support. It looks like there is some built in driver support in ALSA, but I'm not sure if this is true. If not I will need to get a driver for it and I have found none. Any suggestions?

ラベル(1)
0 件の賞賛
返信
1 返信

1,230件の閲覧回数
mendelbullex
Contributor III

OK, so it appears that the linux kernel has a driver for AC97 using PCI. Does nayone know if there is an interface that allows the mcf5445x to use this driver or another similar one with the SSI bus?

0 件の賞賛
返信