5329EVB, new LTIB and 3 serial ports - USB problems?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

5329EVB, new LTIB and 3 serial ports - USB problems?

1,746 次查看
jpa
Contributor IV
When I boot the 5329EVB with the latest LTIB, I notice that all three UARTS are recognized.

My memory is a bit fuzzy, but when I tried enabling that third port (ages ago), I found that one of the third port UART signals (TX or RX) was also being used to control something on the USB port, and so USB operation became unreliable.  USB worked sometimes on one EVB, but not on another.  As I recall, the problem went all the way back to the SOM module, so there was little hope of fixing it if I wanted to use the SOM. 

Did someone find a way around the problem?  Or could someone at Freescale have made the same mistake I did, and that's why I'm having USB problems again?

John
标签 (1)
0 项奖励
回复
1 回复

970 次查看
jpa
Contributor IV
I went back through my notes from the time I was working on the third UART...I was trying to enable the third port while keeping CAN and USB capabilities.  I wasn't able to get that working because one of the pins - mapped to MFP09 - is used as an OE for a buffer on the SOM. 

It's possible the third port is being mapped through the CANRX/TX multifunction pins.

Still trying to get my USB flash stick recognized. 

John
0 项奖励
回复