5275 USB device initialization

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

5275 USB device initialization

2,753 Views
ahjort
Contributor I
I'm having a problem initializing the USB device for the 5275.  Following the steps in the reference manual,
I first configured GPIO for USB.
Then I issued a device reset.
I downloaded the stringBufs, CfgBufs and EpBufs(one EpBufs per logical endpoint, total of 4).  After downloading these, I wait for the USB_DAR[CFG] bit to clear, and it never does!! 
Any help would be appreciated, I'm pretty desperate at this point!  BTW, I'm using the 5275 eval board.
Labels (1)
0 Kudos
Reply
1 Reply

1,328 Views
AWattsMicrium
Contributor I
Im working on the same board and i noticed that you were downloading the configuration data before you wait for the USB_DAR[CFG] to assert, I wanted to know if you ever got the initilization to work because thats what im in the process of doing.
0 Kudos
Reply