52259 wont boot without bdm attached?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

52259 wont boot without bdm attached?

1,576 Views
Byra
Contributor I

Ive got a 52259 on a custom board that boots and runs fine from codewarrior with the bdm attached. However, when I remove the bdm and reset the board, it doesnt run. Im using a 48mhz crystal and it should work with clkmod0 and 1 pulled up to vcc. However, have tried all configurations of clkmod0 and clkmod1 with no luck. When I try the same code on the tower board, it works find and boots up with or without the bdm attached. I have the same 4 pins pulled upon my bdm connector as on the tower board. Im using the same crystal as on the tower board. I dont get it. Im sure its something obvious, but I cant find it.

 

Thanks for any help!

 

--Byra

Labels (1)
0 Kudos
Reply
1 Reply

1,183 Views
scifi
Senior Contributor I

It could be the same problem as this:

 

https://community.freescale.com/message/65237#65237

0 Kudos
Reply