52223 EVB Clock and USB Example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

52223 EVB Clock and USB Example

2,132件の閲覧回数
Bartington
Contributor I
hello all
 
I've check the forum for usb examples as i'm starting to implement the usb on my EVB52223.
I downloaded the HID example and tried to understand it (no mention of the clock in the usb part of the ref manual...Why?).
 
The HID example states that the clock needs to be sorted before the actual example....
Where do we set the clock for the USB Module?
In my particular application i need the uPro to run at max speed so can i still do that and run the USB Port?
Is that also possible to use the internal clock for running the USB Port ?
 
Thanks a lot for your time.
 
Olivier
ラベル(1)
0 件の賞賛
返信
1 返信

1,405件の閲覧回数
Bartington
Contributor I
Me Again
 
I take it back i should have read the ref Manual More Carefully cause i missed the USB_CTRL register where you can select your clock Source. my apology
 
Olivier
0 件の賞賛
返信