52223 EVB Clock and USB Example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

52223 EVB Clock and USB Example

2,102 Views
Bartington
Contributor I
hello all
 
I've check the forum for usb examples as i'm starting to implement the usb on my EVB52223.
I downloaded the HID example and tried to understand it (no mention of the clock in the usb part of the ref manual...Why?).
 
The HID example states that the clock needs to be sorted before the actual example....
Where do we set the clock for the USB Module?
In my particular application i need the uPro to run at max speed so can i still do that and run the USB Port?
Is that also possible to use the internal clock for running the USB Port ?
 
Thanks a lot for your time.
 
Olivier
Labels (1)
0 Kudos
Reply
1 Reply

1,375 Views
Bartington
Contributor I
Me Again
 
I take it back i should have read the ref Manual More Carefully cause i missed the USB_CTRL register where you can select your clock Source. my apology
 
Olivier
0 Kudos
Reply