5207 Chip configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

5207 Chip configuration

2,665 Views
AndyDaytona
Contributor I
Hello,
 
I am currently moving our design from the 5206e to the 5207 and I have a question
about the chip configuration module.
 
I look at the schematics of the evaluation board and I see that the configuration
bits are set using a latch connected to the bus.
 
Is it not possible to use pull ups and downs directly connected to the data bus to
configure the chip? Or is there some problem that I'm not aware of?
 
My bus is already heavily loaded with memory and devices so I am hoping to get rid of this extra load.
 
best regards
Andy
Labels (1)
0 Kudos
Reply
1 Reply

1,442 Views
timotay01
Contributor I

Your using /RCON pin in conjunction with your resistors? See "Reset Configuration" (Section 9.4.1 in the spec I have).

0 Kudos
Reply