16 bit PWM on 64 pin MCF52221CAE?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

16 bit PWM on 64 pin MCF52221CAE?

1,993 次查看
RichTestardi
Senior Contributor II
Hi,
 
Does anyone know if I can use the PWM timers in 16 bit (concatenated) mode on the (pin-limited) 64 pin MCF52221CAE?
 
The reference manual says that when the timers are operated in 16 bit (concatenated) mode, that the outputs are available on pins PWMOUT7, 5, 3, and 1.
 
But the (pin-limited) 64 pin MCF52221CAE only seems to have pins bound to PWMOUT6, 4, 2, and 0 (at pins DTIN3, 2, 1, and 0).
 
Thanks!
 
-- Rich
 
标签 (1)
0 项奖励
回复
2 回复数

1,143 次查看
JimDon
Senior Contributor III

I am afraid your assessment is 100% correct - you can't use the 16 bit mode on this chip.

You will have to do it manually, perhaps using a PIT or a DTIM.

 


0 项奖励
回复

1,143 次查看
RichTestardi
Senior Contributor II
Thanks!!!  I'll be able to get by with 8-bit mode.
 
-- Rich
 
0 项奖励
回复