How to assign a data segment of a c file to a specific location in an l3k file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to assign a data segment of a c file to a specific location in an l3k file

ソリューションへジャンプ
13,242件の閲覧回数
yeyuan1
Contributor III

hello everyone

            The platform I use is B4860。

 

            My requirements are as follows:

            I want to define the data segment in the alloc.c file to a fixed section of memory that is unique to alloc.c.

 

             The normal data segment is defined as follows:

              descriptor__ddr__cacheable_wb__sys__private__data {
                             .struct_start
                             .ddr__cacheable_wb__sys__private__data
                             .bsstab
                             ".c?_bss_sections_table"
                             .init_table
                             .rom_init
                             .rom_init_tables
                             .exception
                             .exception_index
                             .staticinit
                             .zdata
                             reserved_crt_tls
                            .data

                            .mydata
                            .ddr__cacheable_wb__sys__private__rom
                            //LNK_SECTION(heap, "rw", _HeapSize, 0x8, "heap");
                            .bss
                            .ddr__cacheable_wb__sys__private__bss
                  } > ddr_private_data_c_wb;

                A lot of data from c files will be output to this data segment

 

               This is not what I want

 

              I want the data section of the alloc.c file to be exported to mydata,the data segment of any other file cannot be exported to mydata.

 

               What should I do, please?    Or is there a reference document?

 

Thank you all

0 件の賞賛
返信
1 解決策
13,184件の閲覧回数
yeyuan1
Contributor III

My requirement can be achieved with the following method

RENAME "*rtlib_be_x.elb(alloc.eln)", ".text", ".lib_text"

This sentence means Define the code segment of alloc.c to the section's .lib_text

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
13,185件の閲覧回数
yeyuan1
Contributor III

My requirement can be achieved with the following method

RENAME "*rtlib_be_x.elb(alloc.eln)", ".text", ".lib_text"

This sentence means Define the code segment of alloc.c to the section's .lib_text

0 件の賞賛
返信
13,200件の閲覧回数
yeyuan1
Contributor III

 

Can you give me some more advice?

 

thank you

0 件の賞賛
返信
13,194件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

In CodeWarrior for PA 10.5, please create a bareboard project for B4860QDS from File->New->CodeWarrior Bareboard Project Wizard, then build this project from Project->Build Project.

Please refer to __CTOR_LIST__ and __CTOR_END__ definition in section ".ctors" in file __start_e6500_32bit_crt0.c.

Please refer to section ".ctors" definition in LCF file B4860QDS_gcc-aeabi_SMP_ROM.lcf.

0 件の賞賛
返信
13,208件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the section "Additional Small Data Sections" in the attached document.

0 件の賞賛
返信
13,204件の閲覧回数
yeyuan1
Contributor III

 

Thank you for your answer, but this may not meet my needs

 

The documentation describes it as follows.

1.PNG

As you can see from the documentation, this way is defining the x variable to the .red piece of memory, which is not the problem I need to solve.

 

I need to define the data in the C standard library file alloc.c to a specific memory. The c standard library file cannot be modified, so it can only be modified by the l3k file.

 

Other platforms are implemented as follows:

outsection {

     alloc.obj(.data)

 } > mydata

 

Other platforms are implemented in such a way that the data in alloc.c is defined to mydata.

 

So please ask the B4860 if it can achieve such a function?

 

Thanks again for your answer

 

Please help me to solve this problem

0 件の賞賛
返信
13,210件の閲覧回数
yeyuan1
Contributor III

 

                Please help me to resolve this issue.

thank you

0 件の賞賛
返信