CW starcore - ccs core not supported issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW starcore - ccs core not supported issue

1,723件の閲覧回数
sivakumarnm
Contributor I

Hi,

 

I'm trying to execute SDOS project file using Codewarrior 10.1.3 IDE and ONCE USB TAP emulator on MSC8156AMC-SA in an windows XP system. But i'm seeing always "CCS Protocol - CCS core not supported" error and i can't able to execute the project files.

 

Please let me know what could be the issue and how to fix it?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,349件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hello,

My first suggestion would be to upgrade to a newer version of CW. The latest one is here:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-STARCORE-DSP10&tid=CWH

The MSC8156AMC is made of 3 MSC8156. In order to connect to such board, you need a special JTAG configuration file. You can find one here: {CW install dir}\SC\StarCore_Support\Initialization_Files\JTAGConfigFiles\MSC8156AMC.cfg

This JTAG configuration file needs to be added into the Debug Configuration at the Target Type Edit Box.

Hope this helps!

Daniel