using USB TAP Once with ColfFire

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

using USB TAP Once with ColfFire

2,344 Views
Chr_ROTRONICS
Contributor I
We were using before the 56800/E Family DSP with Code Warrior and a USB TAB Once probe.
We are now starting a new project with a 68K/Coldfire MCF52235.
Can somebody tell me if I can modify my USB TAB Once probe to be using with the 68K/Coldfire?
- Do I have only to change the 14pins connector and the ribbon by a 26pins? (On the PCB of the board there is 4 footprints for 4 differents connectors and J5 is a 26pins.)
- Do I have the download a new firmware on the probe?
- Is it possible?
 
Tanks you for help.
Labels (1)
0 Kudos
Reply
1 Reply

1,053 Views
CrasyCat
Specialist III
Hello
 
No you cannot change the firmware and cable in a USBTAP to connect to another CPU.
 
You need to purchase a CWH-UTP-CF-HE to debug on Coldfire.
 
CrasyCat
0 Kudos
Reply