the hardware breakpoint can't be hit in debugging windows

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

the hardware breakpoint can't be hit in debugging windows

1,650件の閲覧回数
joshuali
Contributor I
Category: Technical Request Topic: CodeWarrior Target: PowerQUICC (8xx, 82xx, 83xx, 8 Product: CW for Power Architecture Root Cause/Nature: Feature Request RTOS: Embedded Linux Major: 8 Minor: 8 Patch: 3 Component: Debugger Host: Win XP Type: Query Defect/Enhance #: - Severity: Critical Subject:

the hardware breakpoint can't be hit in debugging windows

the board is MSC8144ADS  From freescale,cpu is MPC8560

Description:

When I Debug the U-Boot Bootstrap Firmware following the step on Pro & Linux App Edition Targeting Manual.pdf page 210,it's seemed everything is ok , but when I set hardware breakpoint in debugging windows, then run it,the breakpoint is not be hit,I want to know what's maybe wrong? 

When create new project with 8144ads template to debug,the hardware breakpoint is ok to hit, 

Thanks.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,056件の閲覧回数
J2MEJediMaster
Specialist I

I am not sure on what you are asking here. Is this supposed to be an actual feature request? If so, you need to enter it through the Service Request page.

 

---Tom

0 件の賞賛
返信