exception unhandled MPC5200B

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

exception unhandled MPC5200B

2,405件の閲覧回数
admin
Specialist II

Hello,

 

    i don' t Know why but if i copy something on a particular part of the external ram on a MPC5200  my debug stops and i read a message dialog on CodeWarrior with the caption "exception unhandled power pc". I speak about the part of ram whose address  is next to 0x1003600, i've 32 M in my HW from 0x00000000 to 01ffffff, i work with a  stand alone application(made by me) that is really small and should'n cover that memory area.

 

Has anybody any idea?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,611件の閲覧回数
ronco
NXP Employee
NXP Employee

My first guess is that the MMU (Memory Management Unit) has not been configured to define this failing address space as valid.  Check your Chip Select, BAT and TLB registers to make sure they're correct.  Also, while the debugger is running, open a Memory window (Data->View Memory) on 0x1003600 (or similar) address and see if you can manually poke new values into this RAM.  And finally, I recommend creating a Memory Configuration file (selected in the 'EPPC Debugger Settings' panel of your CodeWarrior project) to declare the valid and invalid memory spaces in your target's memory map.  This helps the debugger understand what memory spaces are valid and invalid, and the properties (bus-width, address-translations, etc.) associated with each block of addresses.  Details on the 'Memory Configuration' file are found in the "Targeting Manual" in your CodeWarrior's /Help folder.

 

And it's always a good idea to have valid Exception Handler code for every Exception defined for the Power Architecture processor you're debugging.  These Exception Handler routines don't have to do anything more than have a few NOPs and an RTI.  The purpose here is to avoid the processor throwing an Invalid Instruction Exception when it tries to fetch the first Exception Handler instruction, thereby avoiding an unnecessary complication when drilling into the underlying cause of what might be going wrong on your target board.

0 件の賞賛
返信