Which CW suite?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which CW suite?

1,341件の閲覧回数
horia
Contributor I

Hi,

I want to change from gdb on Linux PC to CW on Windows PC platform.

-my C applications run under real time RTEMS OS on PPC processors (MPC8xx now, 

 MPC8XXX in the future).

-I have to use the gnu gcc compiler since RTEMS comes with the appropriate gnu tools versions.

-I'm using in-house built boards.

-I use the BDM debug port (OCD).

Is BASIC suite OK or do I need the STANDARD?

Thanks in advance!

 

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

877件の閲覧回数
J2MEJediMaster
Specialist I

Go to the product web page for the Power Architecture suite and download the Quick Reference Guide for CodeWarrior Suites, which is a PDF (Acrobat) file. You can check to see which suite best meets the requirements for your project.

 

---Tom

0 件の賞賛
返信