W25Q16DW Flash Programmer for ls1012a

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

W25Q16DW Flash Programmer for ls1012a

1,617件の閲覧回数
ruslanfilipovic
Contributor I

We are building a custom board with an LS1012a processor and an attached W25Q16DW QSPI flash.  As a programming algorithm, we used W25Q64F.xml. We added flash device (see attach: W25Q16DW.xml) and fixed the target initialization script (see attach: aktau-target-init.script). In the current moment "dump"  command from device is working, but erase and program command not working. See this image:
179278_179278.pngexample.png

 

Below is the flash connection:
179345_179345.pngsxematic.png

Please, help me fix this problem

Original Attachment has been moved to: W25Q16DW.xml.zip

Original Attachment has been moved to: aktau-target-init.script.zip

ラベル(1)
0 件の賞賛
返信
0 返答(返信)