Reading DIMM SPD using CW 10.5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reading DIMM SPD using CW 10.5

1,965件の閲覧回数
sureshk
Contributor II

Hi,

      I am planning to generate DDR configurations by reading DIMM SPD in Codewarrior eclipse 10.5 version. I am using CWTAP USB version. Kindly help me with  the probe type ID i have to provide in the below screenshot.

 

 

152710_152710.pngpastedImage_0.png

 

      and clarify , how JATG will read SPD ? does it require to load basic .tcl before reading SPD?

 

Regards,

  suresh

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,803件の閲覧回数
addiyi
NXP Employee
NXP Employee

If you are using CWTAP over usb, and this is the only tap probe connected to your machine, is not required to enter any TAP ID. Just select Probe: CWTAP and click on Read SPD.

SPD data is read from the DIMM using an application which is running when Read SPD button is press. This process is transparent for users.

Adrian

0 件の賞賛
返信

1,803件の閲覧回数
sureshk
Contributor II

Thank you Adrina. It is reading SPD even if i leave probe ID blank.

Regards,

  suresh kalepu

0 件の賞賛
返信