RAM variables re-declared at power ON

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RAM variables re-declared at power ON

1,660件の閲覧回数
LordMark
Contributor IV

Hi. I need to keep the value of some RAM variables after a power loss. I obviously have to use a back-up battery. But I have a doubt. Please consider the following example code:

 

int a; <-- global variable

 

main()

{

... 

a = 10;

...

} 

 

Suppose that power goes down and a = 10. What happens after the new power-on with the declaratione int a? Is the variable "a" redeclared? Would its value be lost?

I'm using the MCF52259DEMOKIT; VSTBY pin is connected to 3.3V but after a reset my variable goes to "0" after it is redeclared. 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,013件の閲覧回数
kef
Specialist I

You meant reinitialized, not redeclared, right?

 

C compiler has to initialize all static variables at startup. Static variables without initializer are initialized to zero. All variables in .bss sections are reset to zero at startup. All variables in .data (variables with initializers) are initialized with data from ROM .idata section or something like that. I'm not sure about all sections, but you could move some variables to non default section and startup routine will be unable to initialize those variables.

 

In CW for MCUs V6.3 this seems to be working: 

 

1) Create some custom memory section. Let us call it .noinit

 

Add to lcf file, somewhere between .bss {} block and .custom {} block something like this:

 

  .noinit :
  {
      *(.noinit)
  } >> userram

 

2) In your "C" file 

 

   2.1) make compiler see .noinit section:

 

#pragma define_section noinit ".noinit" far_absolute

   2.2) move varible to .noinit section:

 

__declspec(noinit) int a;

0 件の賞賛
返信