Production Programming support for LS1046A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Production Programming support for LS1046A

1,508 Views
josephwhite
Contributor I

I am looking for third party support for programming LS1046A NOR flash via JTAG using a lower cost and more friendly   automation than Code Warrior suite

Any Suggestions?

My alternative so far:

Segger - Not available yet but is planned 

PE Micro - Has anyone used? Looking at this now.

Labels (1)
0 Kudos
Reply
1 Reply

1,244 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Joseph White,

Previously we have the solution to use CodeWarrior TAP to work with gdb to do the custom board bringing up, please refer to How to debug LS1046A using CodeWarrior TAP and gdb? .

However there is no initialization file for LS1046(ARM processor) in the demo package, you need to create the target initialization file by yourself.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply