Production Programming support for LS1046A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Production Programming support for LS1046A

1,503件の閲覧回数
josephwhite
Contributor I

I am looking for third party support for programming LS1046A NOR flash via JTAG using a lower cost and more friendly   automation than Code Warrior suite

Any Suggestions?

My alternative so far:

Segger - Not available yet but is planned 

PE Micro - Has anyone used? Looking at this now.

ラベル(1)
0 件の賞賛
返信
1 返信

1,239件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Joseph White,

Previously we have the solution to use CodeWarrior TAP to work with gdb to do the custom board bringing up, please refer to How to debug LS1046A using CodeWarrior TAP and gdb? .

However there is no initialization file for LS1046(ARM processor) in the demo package, you need to create the target initialization file by yourself.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信