Porting Tip: possibly unassigned ISR handler

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Porting Tip: possibly unassigned ISR handler

2,514件の閲覧回数
Lokutas
Contributor I
Hello community...
 
When "hand-porting" a S08 QE project to a Coldfire V1 QE project I get the following message.
 
Porting Tip: possibly unassigned ISR handler
 
for all my ISRs, why is this?
 
Help and hints welcomed.
 
Thanks,
Carlos
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,577件の閲覧回数
stanish
NXP Employee
NXP Employee
I'd suggest you to check all of your ISRs. Are all of them assigned to appropriate vector?
e.g in case your original HC08 interrupt routine is declared as:

void interrupt MyISR(void)
{
....
}


and the routine is assigned to appropriate interrupt vector in the original .prm file e.g.

Vector 13 MyISR

then this information is not passed into CFv1 project and a  "Porting Tip" may be generated.
It's recommended to use rather:

void interrupt VectorNumber_Vspi1 MyISR(void)
{
...
}
0 件の賞賛
返信