MPC55xx CW 1.5v problem to use USB-ML-PPCNEXUS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC55xx CW 1.5v problem to use USB-ML-PPCNEXUS

3,444件の閲覧回数
krish_free
Contributor I
Hi, I am facing problem to attach the USB-ML-PPCNEXUS with codewarrior MPC55xx version 1.5. This version of codewarrior doesn't have support for the USB it has only parallel port support for P&E NEXUS. Please help me out on how to connect the USB-ML-PPCNEXUS. I need to use 1.5 version since my code compile only with that version of CW ( due to assembly stuff). I am using MPC5567EVB as the target board, and the debugger also supplied along with that.

Pls let me know soon, Thanks
ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,975件の閲覧回数
stanish
NXP Employee
NXP Employee
Hello krish_free,

CodeWarrior for MPC55xx v1.5 indeed doesn't support USB-ML-PPCNEXUS.
I'd suggest you to try to integrate P&E debugger with CodeWarrior v1.5.
In case you have installed newer codeWarrior e.g. v2.3 the 3-rd party P&E debugger is installed together with CW ("c:\Program Files\Freescale\CodeWarrior for MPC55xx V2.3\pemicro\cw_icdppcnexus.exe" ).

Here are the integration steps:
1. Open Project Settings (ALT+F7)
2. In the "Target" section select "Build Extras"
3. Check the box "Use External Debugger"
4. Enter path to the P&E debugger into "Application" Edit box. e.g. (C:\Program Files\Freescale\CodeWarrior for MPC55xx V2.3\pemicro\cw_icdppcnexus.exe)
5. Enter  "Arguments" according to the setting of your target. e.g.

 "internal FLASH.out" LOADTOFLASH -RESETFILE "mpc5500_booke.mac"
or
 RAM.out LOADTORAM -RESETFILE "mpc5500_booke.mac"

6. set "Initial directory" e.g. "{Project}bin"

Now the debug button should run P&E debugger.

Note:
CodeWarrior v2.x Special Edition includes just starter edition debugger that allows you to debug just 128kB of code.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-SUITE-SPECIAL



0 件の賞賛
返信

1,975件の閲覧回数
changj
Contributor I

你好,我的电脑驱动usb-ml-ppcnexus(fs)rev a显示感叹号,找不到烧写器,系统是WIN7

0 件の賞賛
返信