MPC5534 + P&E USB Multilink flash programming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5534 + P&E USB Multilink flash programming

1,149 Views
Briag
Contributor I

Hello,

 

I just want to know if the issue below is knowed :

 

I can flash a my application on my board on the mpc5534, with the USB multilink except when the aggressive_inline option is set.

(in the preprocessor tab, I've set : #pragma aggressive_inline on )

The error messages are really not explicit.

 

With a Lauterbach interface it is ok, with a CAN reprogrammation (through a bootloader) it is ok.

 

Does someone get the same issue?

 

Regards,

Briag, Automotive, Toulouse, France

Labels (1)
0 Kudos
Reply
1 Reply

898 Views
stanish
NXP Employee
NXP Employee

Hello Briag,

 

This is really weird issue. Assume you build with CodeWarrior.

Which version of CodeWarrior are you using? (Menu Help -> About ->Installed Products)

 

If I understand this issue correctly:

- you are able to build the application with aggressive_inline option set (no link errors).

- then you can program generated flash image (.elf) into controller MPC5534 using Trace32.

- you are unable program the same image into controller using P&E ICD. Error during Flash programming?

 

Could you post an P&E Flash programming error screenshot?

 

 

Stanish

0 Kudos
Reply