M52259Demo MQX_3_7 - Flash Programmer: The Debugger can not write to memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

M52259Demo MQX_3_7 - Flash Programmer: The Debugger can not write to memory

1,195件の閲覧回数
PavelPin
Contributor I

Configuration:

Win 7 Prof

CodeWarior 7.2 Eval.  + Patch 722

Project MQX + MFS (I also tested "only MQX")

Flash Programer :

52259 / Coldfire v2-v4 JM60 OSBDM

Target inic ...ColdFire_Support\Initialization_Files\M52259DEMO.cfg

Erase Flash  :  Erase Command Succeeded  

Blank Check Completed Successfully 

--------

Program/Verify

...MQX_3_7Test_MFS\output\intflash_d.elf.S19

Program

Downloading 0x00010000 bytes to be programmed at 0x00000420 

The Debugger can not write to memory

How to ?

 

Thank Pavel

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,007件の閲覧回数
PavelPin
Contributor I

Hi

For example, FreeRTOS ok writed to internal Flash.

0 件の賞賛
返信