M52233DEMO board problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

M52233DEMO board problem

1,696 Views
yucheng
Contributor I

I build the evaluation project with code warrior for this board, but got problem for debug, program not stop even set breakpoint at start of main(). Do I need to do any environment settings before debug?

btw, for this board, what's the settings for flash programmer?

Labels (1)
0 Kudos
Reply
1 Reply

988 Views
MCF52233
Contributor III

hi yucheng,

which eval project u tried??

what is the size of ur code??

if it is greater than 32K then u hv to target for flash.i.e 1st program the KIT then start debug.

0 Kudos
Reply