How to get licensed? CW 2.8 working with full version of P&E Multilink debugger?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to get licensed? CW 2.8 working with full version of P&E Multilink debugger?

532 Views
NNeff
Contributor III

We are running licensed, dongle'd CodeWarrior 2.8 for MPC5554, and using the P&E Multilink with the debugger within CodeWarrior.  We have updated to the latest P&E drivers (v.10). The host OS is Windows 7.

 

We have three machines running CW 2.8, two with Windows 7 and one under Windows XP.  The installations on one with Win7 and the one with XP both work fine.  On the third, also Win7, the license for CodeWarrior is acting flaky:  FlexLM doesn't show the dongle ID when run from the hard drive, but does when the same executable is run from a thumbdrive.  CW 2.8 won't run without the dongle, but when it starts a splash screen comes up with the message that today is the last day of the demo version and to register a licensed version.  This goes away after clicking "register later" and CW 2.8 appears to work fine, with one problem:

 

We are also running the P&E Debugger code from within CodeWarrior, successfully on the other two machines.  On this third machine, the P&E debugger screens come up with a window title saying it is the "Starter" edition, and won't flash our program because there are "too many lines of code" for a "demo version".  This same P&E Debugger was working fine with the demo version of CodeWarrior 2.8 on this same PC. 

 

I think the problem is with the licensing problems with this installation of CW. (Yes, we have tried reinstalling CW, several times--before and after P&E driver update. The permanent license file for CW looks fine, including HOST_ID=DONGLE_ID=nnnnnn.)

 

Any ideas?  Thanks,

Nancy

Labels (1)
0 Kudos
Reply
1 Reply

330 Views
J2MEJediMaster
Specialist I

You will have to submit a service request for a licensing problem. Click here to go to the service request page to do that.

 

---Tom

0 Kudos
Reply