How do you look up bugs?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do you look up bugs?

1,680件の閲覧回数
Harjit
Contributor II
I just installed an update (CW 6.2.1) for CW6.2 and it calls out three bug fixes.
 
MTWX29971:
ColdFire V1 optimizer : modena25 failure,  loop invariant hoisting problem,
opt speed -O >= 2
MTWX29972:
ColdFire V1 optimizer : various failures when replacing function calls with
indriect calls, opt size, -0 >= 2
MTWX30030:
ColdFire V1 optimizer : volatile peephole issue, volatile load not remove
by the store pattern
How do I get details on these bugs (and other)?
 
Thanks.
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

981件の閲覧回数
J2MEJediMaster
Specialist I
Short answer right now is: you can't get at this information.
We are working on a way to make the information available to developers, as it is a common request, and helps with your coding problems.
No, I don't know when this capability will be available.

---Tom
0 件の賞賛
返信