How do I install a matching command converter for trace configuration in P4080?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I install a matching command converter for trace configuration in P4080?

2,332 Views
hymalaibello
Contributor III

Hello, I would like to use a trace configuration for P4080. When I tried to run it, using CodeWarrior TAP  the next error occurred.

 

TRACING WILL NOT BE ENABLED

 

Did not find matching command converter. Present command converters:cc:0 cwtap:00:04:9F:02:BC:5E

 

 

13882_13882.jpgTRACE1.jpg13901_13901.jpgTRACE.jpg

Thanks!

Regards

Hymalai Bello

Labels (1)
4 Replies

2,071 Views
catalindemergia
Contributor IV

Hi,

Please tell us first exactly what version of Code Warrior for PA you are using. (Help/About CW)

Also, I would like to know what version of 4080 you have. Is it a DS board ?

Try first just a simple stationary project without tracing, let's put tracing away for a moment and

see if it works to debug on the board.

regards,

Catalin

0 Kudos
Reply

2,071 Views
hymalaibello
Contributor III

Hi,

- CodeWarrior for Power Architecture

  Version: 10.4.0

  Build Id:140709

P4080DS Expedition: Rev 3.

The simple stationary project works properly without tracing.

Regards,

Hymalai

0 Kudos
Reply

2,071 Views
lunminliang
NXP Employee
NXP Employee

Are you using remote CCS when the error report?

0 Kudos
Reply

2,071 Views
catalindemergia
Contributor IV

ok, now what you have to do is modify this simple stationary project so that it will

support tracing. You can do this from Debug Configuration/Trace and Profile tab

trace_profile.png