For SDK , we use Linux BSPs . What is there in Codewarrior in analogy to the BSPs in SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

For SDK , we use Linux BSPs . What is there in Codewarrior in analogy to the BSPs in SDK

1,079 Views
hammadnayeem
Contributor II

For SDK , we use Linux BSPs . What is there in Codewarrior in analogy to the BSPs in SDK

Labels (1)
0 Kudos
Reply
1 Reply

951 Views
lunminliang
NXP Employee
NXP Employee

Hi,

Sorry not quite understand your question.

In CodeWarrior you could develop and debug bareboard code, also you could debug uboot code or Linux code.

You could find more information in the documents of CodeWarrior installation directory.


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply