Flash programmer does not come up as a possible target task for LS2085A.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash programmer does not come up as a possible target task for LS2085A.

1,408 Views
Suede
NXP Employee
NXP Employee

I am using the following version of CodeWarrior

150043_150043.pngpastedImage_0.png

 

I want to define a target task for flash programming, but I don't get Flash Programmer as a choice.

Only import/Export/Fill Memory comes up in the dialogue box.

 

150065_150065.pngpastedImage_1.png

Labels (1)
0 Kudos
Reply
2 Replies

1,270 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Bo Karlsson,

The procedure for flash programming on LS2085 with CodeWarrior is different with PowerPC or LS1 platform.

After install CodeWarrior for ARMv8, please refer to "Chapter 7 Flash Programmer" in CW4NET_v2016.01\CW_ARMv8\ARMv8\Help\PDF\ARMv8_Targeting_Manual.pdf to do flash programming.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,270 Views
addiyi
NXP Employee
NXP Employee

Bo,

Please use the latest CW for ARMv8 release, and not CW for APP.

Adrian

0 Kudos
Reply