Ext. Flash drivers for M5282EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ext. Flash drivers for M5282EVB

3,377 Views
TTA
Contributor I
Hi,
I am in the process of purchasing the M5282EVB Evaluation Board for the MCF5282 microprocessor.
Do i get  the Flash drivers to write to the External Flash? If so , where can i find it?
Please let me know.
 
Thanks.
TTA
Labels (1)
0 Kudos
Reply
2 Replies

1,737 Views
TTA
Contributor I

Hi,

Thanks. The M5282EVBUM.pdf gives the information that the flash device is Am29lvl60DB and also to "Refer to the specific device data sheet and sample software provided for configuring the flash memory". Is the software same as the flash driver or is it something else. If its not, will i get some application notes or some documentation that i can use to write to the flash device? 

Regards,

TTA

0 Kudos
Reply

1,737 Views
Technoman64
Contributor III
0 Kudos
Reply