Ext. Flash drivers for M5282EVB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ext. Flash drivers for M5282EVB

3,371件の閲覧回数
TTA
Contributor I
Hi,
I am in the process of purchasing the M5282EVB Evaluation Board for the MCF5282 microprocessor.
Do i get  the Flash drivers to write to the External Flash? If so , where can i find it?
Please let me know.
 
Thanks.
TTA
ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,731件の閲覧回数
TTA
Contributor I

Hi,

Thanks. The M5282EVBUM.pdf gives the information that the flash device is Am29lvl60DB and also to "Refer to the specific device data sheet and sample software provided for configuring the flash memory". Is the software same as the flash driver or is it something else. If its not, will i get some application notes or some documentation that i can use to write to the flash device? 

Regards,

TTA

0 件の賞賛
返信

1,731件の閲覧回数
Technoman64
Contributor III
0 件の賞賛
返信