Error installing USB drivers for CodeWarrior Probes. Both the initial install and the manual process fail. This is on Windows 7.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error installing USB drivers for CodeWarrior Probes. Both the initial install and the manual process fail. This is on Windows 7.

1,262 Views
jamesros
Contributor I


I was trying to install "CodeWarrior for PowerArchitecture (Eclipse-Windows Hosted) v10.4.exe"
I am running on Windows 7.

The install was run as administrator.

I have tried it several times.

The status on the Installation Wizard just says "Install failed" Is there any way to get more information?

Labels (1)
0 Kudos
Reply
1 Reply

1,061 Views
lunminliang
NXP Employee
NXP Employee

Hello James Ros,

Is this error of CodeWarrior installation error or USB driver installation error?

Did you follow the steps in the driver read me file:

C:\Freescale\CW_PA_v10.4.0\PA\ccs\drivers\usb\readme.txt

Regards

Lunmin

0 Kudos
Reply