Does flash programmer work on MCF52223?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does flash programmer work on MCF52223?

ソリューションへジャンプ
2,596件の閲覧回数
jonathang
Contributor II

Has anyone out there ever gotten the CodeWarrior Flash Programmer tool to work on the internal flash in the MCF52223?  I'm using the CW special edition 7.2 at the moment, but have never gotten the flash programmer to work.  I've tried lots of different configuration tricks, but the RAM download always fails.  I have no problem downloading code into RAM through the normal Project/Run function, and I can read and write memory freely for debugging.

 

I've been using CFFlasher to burn flash, and it works, but it takes an annoying lot of mouse-clicks each time.  CFFlasher seems to have a partly-implemented command line mode that doesn't work.  It would be great if someone would finish that, or release the source code to the user community so that we could get it working.

 

What I'd really like to do is use the CodeWarrior Flash Programmer and then write a script to automate the erase/program cycle so I could get something close to a one-click solution. 

 

This single issue makes CodeWarrior very cumbersome to use with MCF52223 when code sizes exceed what can be debugged in RAM.  I keep feeling like I must be missing something.  Looking through the forums has not enlightened me.  What's the scoop on this?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,740件の閲覧回数
jonathang
Contributor II

I seem to have solved my problem.  It was caused by the fact that CodeWarrior uses an old version of the file unit_cfz.dll (from July 23, 2007).  The CFFlasher program uses a slightly different version (March 4, 2007), and some P&E Micro tools install a much newer version (November 11, 2009).

 

The issue is discussed on pemicro's forums here.  Following the directions at http://www.pemicro.com/faqs/faq_view.cfm?id=103 fixed it. 

 

I made sure that only the 2009 version of unit_cfz.dll was in the CodeWarrior, CFFlasher, and windows/system32 directories.  My problems with the flash burner disappeared.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,741件の閲覧回数
jonathang
Contributor II

I seem to have solved my problem.  It was caused by the fact that CodeWarrior uses an old version of the file unit_cfz.dll (from July 23, 2007).  The CFFlasher program uses a slightly different version (March 4, 2007), and some P&E Micro tools install a much newer version (November 11, 2009).

 

The issue is discussed on pemicro's forums here.  Following the directions at http://www.pemicro.com/faqs/faq_view.cfm?id=103 fixed it. 

 

I made sure that only the 2009 version of unit_cfz.dll was in the CodeWarrior, CFFlasher, and windows/system32 directories.  My problems with the flash burner disappeared.

0 件の賞賛
返信
1,740件の閲覧回数
J2MEJediMaster
Specialist I

Try searching for "MCF52223" and "flash" in the search function at the upper right of this web page. You'll get a number of hits, and one of them might have an answer to your problem.

 

---Tom

 

0 件の賞賛
返信