Device Cfg File For The Micron Flash On The TWR-MPC5125

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Device Cfg File For The Micron Flash On The TWR-MPC5125

1,507件の閲覧回数
Tim562
Senior Contributor I

Hi All,

 

    Does anyone have access to a FPDeviceConfig.xml file for CodeWarrior For MobileGT 9.2 that includes the flash device on the Freescale TWR-MPC5125 module? The flash device is a Micron 29F32G08CBABA 32 GB NAND Flash chip and it's not included in the C:\Program Files\Freescale\CodeWarrior for MobileGT V9.2\bin\Plugins\Support\Flash_Programmer\EPPC\FPDeviceConfig.xml file that CodeWarrior uses to specify the flash devices it can access. Failing that does anybody know of another way to program the flash device on these modules? Thanks!

 

Best,

Tim

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,139件の閲覧回数
martonmiklos
Contributor I

Hello Tim!

 

Did you get further with your problem?

 

I would need support for the MT29F4G16 device with MPC5125.

I analyzed the FPDeviceConfig, and found the entry to be most similar. I have tried to create a flash description xml using the flashgen_entry.pl, but when I select the created flash device the CW simply hangs.

 

Thanks,

Miklós

0 件の賞賛
返信