Debugger problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugger problems

Jump to solution
4,248 Views
ralu
Contributor III

Debuuging does not work any more for CW 7.1 on MCF52235, because it looks like tha only one interrupt source works.

 

I can put one breakpoint, but after stop i can not make any steps, becuase it lost conenction.

 

 

 

I do not know why, but it can be due to drivers on PC or drivers on Multilink, but how can is solve this issue?

 

EDIT

 

I have two Multilinks Here (rev C and rev D)  I also have two boards to test on. Uploading FW works fine, but debuuging lost connection after first breakpoint.

Labels (1)
0 Kudos
Reply
1 Solution
3,977 Views
ralu
Contributor III

Issue was that due to use of some software from pe-micro debugger got impropper FW.

I got new FW for multilink FE from pe-micro support.

View solution in original post

0 Kudos
Reply
3 Replies
3,977 Views
FridgeFreezer
Senior Contributor I

Are you disabling the PST data pins / setting them to other functions?

/* Enable debug */ #ifdef DEBUG MCF_GPIO_PDDPAR = 0x0F; // PST/DDATA Pins enabled #else MCF_GPIO_PDDPAR = 0; // Disabed - reduces EMC #endif

 

3,977 Views
alager
Contributor II

Is this in the BDM driver somewhere, or just in the code?

We have an issue where the BDM is setting MCF_GPIO_PDDPAR = 0x0F, and we don't want that.

We need to use the PST pins as gpio.

Thanks,

Aaron

0 Kudos
Reply
3,977 Views
ralu
Contributor III

Issue was that due to use of some software from pe-micro debugger got impropper FW.

I got new FW for multilink FE from pe-micro support.

0 Kudos
Reply