Codewarrior v1.7 special edition for ColdFire

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior v1.7 special edition for ColdFire

2,501件の閲覧回数
Prao
Contributor I

I just installed v1.7 of the Codewarrior special edition and downloaded the quick start sample program for MCF52256(ColdFire).

When I tried to debug the program, I got the following error:

 

"Unable to use the plugin "CCS_CF_Protocol_Plugin" It Is
licensed and a valid license key was not found.

 

Can anybody tell me what I should do to eliminate this error?

 

Thanks.

 

Prao

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,417件の閲覧回数
J2MEJediMaster
Specialist I

Check and see if you have a license.dat file in your CodeWarrior installation directory. You need that to run certain features, even for the Special Edition.

 

---Tom

0 件の賞賛
返信

1,417件の閲覧回数
Prao
Contributor I
I did check to see if the license.dat file existed in the installation directory. I even copied it to the project directory just to be sure! It still doesnt debug! Any suggestions?
0 件の賞賛
返信