Codewarrior MPC55xx V5.90 Command line issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Codewarrior MPC55xx V5.90 Command line issue

2,256 次查看
jackzhou
Contributor I
Hello,
 
CodeWarrior MPC55xx,i want to use tcl script,when i
use the command:
cmdIDE /d script.tcl
It prompt:
ERROR:Bad Debug Executable argument (enclose debug-IDE in "quotes").(Code 11)
 
And the script.tcl is:
debug
reset
go
exit
 
Regards,
Jack
标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,234 次查看
Voxan
Contributor III
Hi there,

CW 55xx is special as this tool chain is build only, there is no debugger included in the package.
So any call to the debugger will end like this...

Hope this helps...

Regards
0 项奖励
回复